Multiple secure boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multiple secure boot

1,581件の閲覧回数
DanielePagani
Contributor II

    Dear sirs,

our idea is to save several boot images in Flash (FlexSPI NOR) and to start one or the other under certain conditions.

This project is working fine, however, we're wondering if it is possible to make these boot images safe.

So, the question is whether it is possible to save in Flash (and run as XIP) different boot images with different security (as example one for each image).

BR

Daniele

0 件の賞賛
返信
2 返答(返信)

1,499件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

hello,

What about "different security"? If for different Key it is possiable. It will can't if for secure encryption boot it is not possiable. One may refer to the information as the link.URL:.

NXP-MCUBootUtility/README.md at master · JayHeng/NXP-MCUBootUtility · GitHub 

best regards

TIC

0 件の賞賛
返信

1,499件の閲覧回数
DanielePagani
Contributor II

    Hi fangfang‌,

it seems that NXP-MCUBootUtility is a great tool.

However, it requires image_enc.zip file and it's not possible access to it outside of China.

We're wondering if you can upload it somewhere else.

BR

Daniele

0 件の賞賛
返信