Microcontroller/Microprocessor with two USB HS and 16 endpoints

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Microcontroller/Microprocessor with two USB HS and 16 endpoints

2,169件の閲覧回数
atas2000
Contributor II

Is there a Microcontroller/Microprocessor with two USB HS and 16 endpoints?

0 件の賞賛
返信
1 返信

2,115件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hello Aleksandr,

 

The closest recommendation I can give you from the MCU side are RT1050, RT1060 or RT1064. This MCU includes two USB 2.0 Controller Cores that supports up to 8 bidirectional endpoints each.

 

There are other options such as LPC546XX family or LPC5500 family but these MCUs support only one HS USB module and one FS USB module.

 

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信