MIMXRT685-EVK: Getting debug authentication to work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT685-EVK: Getting debug authentication to work

14,519件の閲覧回数
daparker
Contributor III

Hello, I'm evaluating the debug authentication process in section 48.10 of the RT600 user manual to enable post-launch retail microcontroller debugging for an upcoming product. I'm looking for some pointers or guidance on getting the debug authentication to succeed with with my MIMXRT685-EVK board and NXP tools. So far, I've created the attached project using the MCUXpresso Secure Provisioning SDK 4.1 [secure_provisioning.zip]. This project is configured to create a secure bootable image based on the gpio_led_output demo, write the RKH to OTP, RTKH to shadow registers and disable Hifi4 DSP access unless the debug authentication succeeds. To setup my repro, I use the following steps:

  1. Build the gpio_led_output in MCUXpresso with the  

    BOOT_HEADER_ENABLE preprocessor define undefined. Then build the image in the SP SDK and click "Show write script" to update the write script used below.

  2. Set to enter serial ISP mode. ISP DIP switches (L,L,H)
  3. Remove power from the system to clear shadow register config, then plug the link probe and RT685 USB back in.
  4. Run these scripts to program the image from the Secure Provisioning project:
    1. /write_image_mac.sh

    2. ./gen_scripts/write_shadows.sh

  5. Set to boot from FlexSPI Port B: (H,L,H), soft reset. Verify the target is booted securely into the gpio_led_output demo by making sure the blue user LED is on.

  6. Generate a DC and attempt authentication with the following commands:
    1. nxpdebugmbox gendc -c gendc_config.yaml -e gen_sb/mbi_config.json auth.dc --force

    2. nxpdebugmbox -vv auth -b 0 -c auth.dc -k dck

  7. Authentication fails with the attached log [log.txt]. Exerpt:

INFO:spsdk.debuggers.debug_probe_pyocd:PyOCD connected via LPC-LINK2 CMSIS-DAP V5.224 probe.
DEBUG:spsdk.debuggers.utils:step T.1: Activate the correct AP
DEBUG:spsdk.debuggers.utils:step T.2: Set the AP access size and address mode
DEBUG:spsdk.debuggers.utils:step T.3: Set the initial AHB address to access
DEBUG:spsdk.debuggers.utils:step T.4: Access the memory system at that address
DEBUG:spsdk.debuggers.utils:Chip has NOT enabled AHB access.
INFO:spsdk.apps.nxpdebugmbox:Debug Authentication ends without AHB access.

Is there anyone who can help out with this?

ラベル(1)
タグ(2)
0 件の賞賛
返信
7 返答(返信)

14,486件の閲覧回数
daparker
Contributor III

I have a real JLink. I can just switch to using that instead of the LPC-LINK2. This should be the full set of repro steps now, and both debugger keys should be included. The result is not much different from before, which I attached [nxpdebugmbox.txt]

./write_image_mac.sh
./gen_scripts/write_shadows.sh
nxpdebugmbox -vv auth -b 0 -c auth.dc -k keys/dck.pem

I think my configuration should be correct, however I'd appreciate some help validating it. I noticed some of the stuff in the yaml appeared to be unused by nxpdebugmbox so I removed it, as I'm passing in an elf2sb file instead. Also, this should be a totally unfused MCU. Are any fuses required to be burned or data written to flash to make debug auth work? I don't think that should be the case, but I'd like to double check.

14,455件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @daparker 

Thanks for the additional information! 

I am currently reviewing your files and steps. 

Diego.

0 件の賞賛
返信

14,394件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @daparker 

We would need to burn some fuses to get debug authentication. 

To avoid assumming things, could you help me to read  all the fuses you got on your MCU (if any)?

Many thanks for your patience, 

Diego

0 件の賞賛
返信

14,376件の閲覧回数
daparker
Contributor III

Good morning, we're also suspecting fuse config as we were able to get this to work on one of our proto boards. Attached is the fuse config read from SPSDK.

14,366件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @daparker 

Thank you for your reply!

Our team  double checked the shadow registers required by debug authentication, For SEC_BOOT_CFG[5] (0x40130194), it should be set to 0x80.

We are also checking the reliability of configuration using fuses, I will get back to you as soon I receive more information. 

Regarding your comment on red : we're also suspecting fuse config as we were able to get this to work on one of our proto boards, to avoid assuming anything could you expand on the text on red?

Many thanks for your patience, 

Diego

0 件の賞賛
返信

14,348件の閲覧回数
daparker
Contributor III

Hey Diego, happy Friday. To Clarify in red, I mean we got this working on our own hardware. I'm just not able to get it work on my devkit. Besides that, we would like to use OTP not PUF. I did try your suggestion below and this still doesn't work on my devkit.

14,494件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @daparker 

I hope you are doing well! 

I am concerned about the debug Credential Key you have DCK.pub , I have not find its associated .pem in your files. Or as it is private, did you put it somewhere else? Or did you verified that the .pub you gave us , corresponds to the .pem you have?

diego_charles_1-1660341873529.png

diego_charles_2-1660345602089.png

So what I suggest you to do is: 

 generate debugger key pair ( I have not seen this command yet on your files or description)

nxpkeygen -d debug -k rsa2048 keys\dck.pem

diego_charles_3-1660345643254.png

diego_charles_4-1660345679898.png

 

So, when calling the this command give the dck.pem

nxpdebugmbox -vv auth -b 0 -c auth.dc -k dck.pem

Here is an example with the LPC55 

diego_charles_5-1660345841581.png

Here is another tip:  I recommend you to load J-Link into your  LPC-LINK2. Sometimes when we enable debug authentication, Segger is more reliable to initiate a debug session on the MCUXpresso. I do not why , but I have seen this on the LPC55.

 

Please let me know more details, so we can dig further if needed. Checking if DC keys match to what we expect on the RT600. Or if there is any setting we could do.

All the best,

Diego.