MIMXRT1176 Cannot Boot code using SDRAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1176 Cannot Boot code using SDRAM

ソリューションへジャンプ
2,585件の閲覧回数
razools
Contributor III

Hi,

 

I am unable to bootup code using SDRAM. I am using lwip_dhcp_freertos_cm7 example. Following are my settings:

MCU Settings

MCU SettingsMCU Settings

Preprocessor Settings:PreProcessor SettingsPreProcessor Settings

Linker SettingsLinker SettingsLinker Settings

However, Code Boots up fine I don't link application to RAM. It also works fine when using SRAM_DTC_cm7.

Following is the error I am getting when i hit debug buttonErrorError

0 件の賞賛
返信
1 解決策
2,570件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @razools ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest support, please refer to the post.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,571件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @razools ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest support, please refer to the post.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------

0 件の賞賛
返信
2,556件の閲覧回数
razools
Contributor III

Thanks @jeremyzhou 
with the post you mentioned above 
i am able to bootup my application directly on SDRAM

0 件の賞賛
返信