MIMXRT1064 - any differences between 10x10 and 12x12 package sizes?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MIMXRT1064 - any differences between 10x10 and 12x12 package sizes?

跳至解决方案
1,015 次查看
jason_lo
Contributor II

We previously designed a custom board using MIMXRT1064DVL6A, which is the 10x10 mm package.  Now that the 12x12 mm package is available, we would like to use that instead.  Besides package size, are there any other differences between them?  We have reviewed datasheet and manual and cannot find any differences, but want to double-check.

Regards,

Jason

标签 (1)
标记 (1)
1 解答
956 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Jason,

 

You are correct, there are no differences apart from the package.

 

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored.

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

在原帖中查看解决方案

1 回复
957 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Jason,

 

You are correct, there are no differences apart from the package.

 

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored.

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------