USB-MSD Host not works in EVKB-iMXRT1050

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB-MSD Host not works in EVKB-iMXRT1050

1,862 次查看
sudheer_adigopu
Contributor I

Hi,

I am using "evkbimxrt1050" for testing the USB host SDK example "usb_host_msd_fatfs".

But the example not works. Log info shows "host init done", after that now log. Also the Breakpoints are not hitting after USB insert.

Can anyone help on this.

Regards

Sudheer

标签 (1)
4 回复数

1,742 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hello Sudheer,

 

I have tried to use the example you are referring to replicate this issue on my side. However, device was detected correctly when the USB was attached. Please check my test below.

pastedImage_2.png

I used usb_host_msd_fatfs_bm example from SDK 2.7.0 and MCUXpresso IDE v11.1.1. I ran the example on my MIMXRT1050-EVKB.

 

Best regards,

Felipe

1,741 次查看
mjbcswitzerland
Specialist V

Hi

Are you connecting the memory stick to the correct USB connector? The one furthest away from the Ethernet jack is used for host mode.

To test the HW load the attached binary file which gives USB-CDC device on the first USB device interface and USB-MSD host on the second. This is a standard uTasker configuration, fully encrypted with serial and OTA uploading support built in (see https://www.utasker.com/docs/iMX/uTaskerLoader_TestDrive.pdf for loading and other details) which will allows you to verify that the USB host issue it is not a local board problem.
Command line interface of the debugger's VCOM at 115kBaud or on the USB-CDC device connection:

Eg.

Hello, world... MIMXRT1050 [Power-on]
Static memory = 0x00001d4c
OS Heap use = 0x37e4 from 0xc000
Initial stack margin 0x00051ee0
FlexRAM:
4 Code banks [0x00000000..0x0001ffff]
12 Data banks [0x20000000..0x2005ffff]
SPI Flash: Cypress 64MByte S26KL512
uFileSystem integrity
Start: 0x60100000
Granularity: 0x00040000
End: 0x6127ffff
OK
USB (1) device detected
USB HS device detected
USB device information ready:
USB2.0 device with 64 byte pipe
Vendor/Product = 0x1a19/0x1628
Manufacturer = "Generic"
Product = "Flash Disk"
Serial Number = "090627173229>42"


Bus-powered device (max. 100mA) with 1 interface(s)
Mass Storage Class : Sub-class = 0x06 interface protocol = 0x50
Endpoints:
1 = BULK IN with size 512
2 = BULK OUT with size 512
Enumerated 1 (1)
LUN = 1
UFI INQUIRY -> Status transport - Passed
UFI REQUEST SENSE -> Status transport - Passed
UFI FORMAT CAP. -> S:0x02008140
HS USB error - 1
Stall on EP-1
IN EP-1 cleared
Status transport - UFI FORMAT CAP. -> (2:512:495616) Status transport - Passed
UFI READ CAP. -> (512:495615) Status transport - Passed

Mem-Stick mounting...
Disk E mounted


Serial number: 4294967295-65535
Software version V1.4.012
Device identification: uTasker Number 1


     Main menu
===================
1              Configure LAN interface
2              Configure serial interface
3              Go to I/O menu
4              Go to administration menu
5              Go to overview/statistics menu
6              Go to USB menu
7              Go to I2C menu
8              Go to utFAT disk interface
9              FTP/TELNET commands
a              CAN commands
help           Display menu specific help
quit           Leave command mode
8



  Disk interface
===================
up           go to main menu
info         utFAT/card info
dir          [path] show directory content
dird         [path] show deleted directory content
dirh         [path] show hidden content
infof        [path] show file info
infod        [path] show deleted info
cd           [path] change dir. (.. for up)
comp         compare [file1] with [file2]
file         [path] new empty file
write        [path] test write to file
mkdir        new empty dir
rename       [from] [to] rename
trunc        truncate to [length] [path]
copy         [file1] to [file2]
hide         [path] file/dir to hide
unhide       [path] file/dir to un-hide
prot         [path] file/dir to write-protect
unprot       [path] file/dir to un-protect
print        [path] print file content
del          [path] delete file or dir.
format       [-16/12] [label] format (unformatted) disk
fformat      [-16/12] [label] full format (unformatted) disk
re-format    [-16/12] [label] reformat disk!!!!!
re-fformat   [-16/12] [label] full reformat disk!!!!!
sect         [hex no.] display sector
sectw        [hex no.] [offset] [val] [cnt]
help         Display menu specific help
quit         Leave command mode
>dir
Directory E:\


---A 07.02.2012  02:17          9683567 LanModem_7-2-2012.zip
---A 06.08.2017  19:54          9852838 LAN_MODEM_V2.0.2_9-2-2012.zip
---- 26.02.2012  00:56 <DIR>            2011
---A 03.03.2012  23:58         12459259 STM32_3-3-2012.zip
---A 03.03.2012  23:58         24276760 Kinetis_3-3-2012.zip
---A 04.03.2012  00:00         52577632 Documents_3-3-2012.zip
---- 30.11.2012  03:48 <DIR>            BASIC_V2
---- 01.12.2012  04:03 <DIR>            BASIC_1-12-2012
---- 09.03.2020  12:00 <DIR>            TestDIR
---- 01.12.2012  04:05 <DIR>            AVR32_xplanation
---A 26.10.2015  12:00             2135 opt.txt
---- 02.12.2012  12:44 <DIR>            BASIC_02-12-2012
---A 26.10.2015  12:00            65516 test2.txt
---- 02.12.2012  17:45 <DIR>            BASIC_02-12-2012_2
---A 26.10.2015  12:00            69148 stick.c
---- 09.12.2012  07:42 <DIR>            Basic_9-12-2012
---A 28.05.2020  20:12          9165247 relais_10-4-2013.zip
---- 26.10.2015  12:00 <DIR>            test
---- 21.04.2013  01:24 <DIR>            Docs-April_2013
---- 13.05.2017  06:28 <DIR>            DSP
---- 21.04.2017  01:24 <DIR>            farlight_Net512
---A 11.06.2017  15:05            65516 application.c
---A 11.06.2017  15:48            69148 uFile.c
---A 17.06.2017  01:49             2135 Optionen_d.txt
---A 07.06.2020  16:51            38928 software.bin
13 files with 118327829 bytes
12 directories, 52256768 bytes free
E:\>USB device removed
Mem-Stick unmounted
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Regards

Mark

[uTasker project developer for Kinetis and i.MX RT]

0 项奖励
回复

1,741 次查看
sudheer_adigopu
Contributor I

Hi Felipe,

Thank you for your help, I was actualy trying on J10 connector. I changed the code to work for J10. Now it works fine.

In my cutom board we are using OTG2 (which is same as J10 in EVKB). The same code not working in my custom board. The only harware difference is, we are not using micro USB connector (the regular 4pin USB connector is used).

When I connect USB to board, I was getting "enumeration failed" error on the debug console.

Can you please help me.

Regards

Sudheer

0 项奖励
回复

1,741 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Sudheer,

 

I highly recommend you to check our i.MX RT Hardware Development Guide for the MIMXRT1050/MIMXRT1060 Processor. In this document you will find a chapter dedicated to USB that gives you guidelines that you may find useful and that you should check that you are following in your design. In addition, you can consult IMXRT1050 EVKB schematics for reference.

 

Best regards,

Felipe

0 项奖励
回复