MEGAMIX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
1,230 Views
AndreiZi
Contributor I

Dear Support,

I use RT1172 MPU in my project.

How can I turn off  MEGAMIX, DISPLAYMIX and MIPIPHY domains to reduce the total consumption of the power?

i.MX-RT1170 

Kind regards,

Andrei

0 Kudos
Reply
1 Solution
1,206 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Please refer to chapter 5.3 from this application note:
AN13148: i.MX RT1170 Low-Power Modes – Application Note

The example is set to power off the Wakeupmix at the same setpoint MEGAMIX and DISPLAYMIX are off so it will need to be modified so at a determined setpoint WAKEUP remains on while the rest are off.

Best regards,
Omar

View solution in original post

0 Kudos
Reply
1 Reply
1,207 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Please refer to chapter 5.3 from this application note:
AN13148: i.MX RT1170 Low-Power Modes – Application Note

The example is set to power off the Wakeupmix at the same setpoint MEGAMIX and DISPLAYMIX are off so it will need to be modified so at a determined setpoint WAKEUP remains on while the rest are off.

Best regards,
Omar

0 Kudos
Reply