M.2 BLE modules

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

M.2 BLE modules

Jump to solution
2,980 Views
romitchatterjee
Contributor V

Which M.2 modules have BLE functionality implemented in it? I am using an NXP i.MX RT 1060 EVK.

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
2,869 Views
puja_sah
Contributor II

Hello Romit,

The new SDK 2.6.2 for i. MX RT 1060 EVK includes the BLE functionality for 1DX EVB. Currently, it is implemented in 1DX only but 1LV and 1MW are on the roadmap to have BLE functionality implemented on them.

You can download the SDK from Welcome | MCUXpresso SDK Builder 

For more information about the module, please refer to https://wireless.murata.com/type-1dx.html 

To download the quick start guide for i. MX RT, please refer to this link https://wireless.murata.com/datasheet?/RFM/data/murata_quick_start_guide_freertos.pdf 

Hope it helps.

Thanks,

Puja

View solution in original post

0 Kudos
Reply
2 Replies
2,869 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Romit Chatterjee,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Actually, I'm not very clear about your question, whether you can clarify it again.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,870 Views
puja_sah
Contributor II

Hello Romit,

The new SDK 2.6.2 for i. MX RT 1060 EVK includes the BLE functionality for 1DX EVB. Currently, it is implemented in 1DX only but 1LV and 1MW are on the roadmap to have BLE functionality implemented on them.

You can download the SDK from Welcome | MCUXpresso SDK Builder 

For more information about the module, please refer to https://wireless.murata.com/type-1dx.html 

To download the quick start guide for i. MX RT, please refer to this link https://wireless.murata.com/datasheet?/RFM/data/murata_quick_start_guide_freertos.pdf 

Hope it helps.

Thanks,

Puja

0 Kudos
Reply