List of supported QSPI flash devices

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

List of supported QSPI flash devices

ソリューションへジャンプ
3,532件の閲覧回数
nickwallis
Senior Contributor I

Hi,

Is there a definitive list of supported QSPI flash devices please? This is for using on the flexSPI for booting the IMXRT106x.

Also, can equivalent devices be used as an alternative? By equivalent, I mean both hardware compatible (PCB package and pinout) and software compatible (same command set.)

Does either the chip itself, the SDK or the IDE/flash programming tools check the JEDEC ID of the connected device? (thus preventing an alternative device with a different JEDEC ID from functioning.) Or can any equivalent device be used successfully?

thanks

-Nick

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
3,508件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Nick, 

Please refer to the following application note: 

How to Enable Boot from QSPI Flash (nxp.com)

Section 5 has the information that you are looking for. Table 3 has some memories that we had tested, but be aware of the following information. 

Besides the EVK onboard QSPI Flash, the following Flashes are also supported, and please note those
are just typical examples with those flash vendors, theoretically, we could support all the flash memory
that comply with JESD216/JESD216A/JESD216B.

Regards,
Victor 

元の投稿で解決策を見る

2 返答(返信)
3,487件の閲覧回数
nickwallis
Senior Contributor I

Thanks Victor, that answered my question.

regards

-Nick

0 件の賞賛
返信
3,509件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Nick, 

Please refer to the following application note: 

How to Enable Boot from QSPI Flash (nxp.com)

Section 5 has the information that you are looking for. Table 3 has some memories that we had tested, but be aware of the following information. 

Besides the EVK onboard QSPI Flash, the following Flashes are also supported, and please note those
are just typical examples with those flash vendors, theoretically, we could support all the flash memory
that comply with JESD216/JESD216A/JESD216B.

Regards,
Victor