LPADC1 Differential mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPADC1 Differential mode

ソリューションへジャンプ
4,616件の閲覧回数
Max83
Contributor II

Dear support,

I'm designing a custom board based on IMXRT1176 and I have to configure LPADC1 to take a differential reading through  pins GPIO_AD_06 (A,1_0) and GPIO_AD_07 (B, 1_0). I'm using the MCUXpresso Config Tool under the peripheral section to add a new command. The tool allow me to select Channel sample mode=Differential mode (A as plus, B as minus) and Channel number=A, 1_0 » [N13] GPIO_AD_06 and B, 1_0 » [T17] GPIO_AD_07. The problem is that I have a warning that say Signal channel 1B is not routed. On the Pin section of the tool the LPADC1 is already selected for the pins GPIO_AD_06 and GPIO_AD_07.

Why I have this warning? Am I doing something wrong? Herewith enclosed a screenshot of the tool.

Thank you in advance for the support.

 

Kind regards,

Max83

0 件の賞賛
返信
1 解決策
4,506件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
6 返答(返信)
4,481件の閲覧回数
Max83
Contributor II

Ok, thank you very much for the support.

 

Kind regards,

Massimo

0 件の賞賛
返信
4,587件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @Max83 ,

I tested both on MCUXpresso IDE and config tool. But I didn't see the warning. What's your tool version. I found the item name in Cahhenl number menu is different.

jingpan_1-1680144950453.png

Have you set ADC pins in pin config window like this?

jingpan_0-1680144928185.png

 

Regards,

Jing

 

0 件の賞賛
返信
4,582件の閲覧回数
Max83
Contributor II

Dear Jing,

thank you for your reply.

I'm using MCUXpresso Config Tools Pins version 13 and Peripheral Version 12.0. The SDK in in version 2.13.1.

Yesterday I did some tests with the MCUXpresso IDE and I can confirm that the Channel number conformed with your one. But also in this tool I have the same problem.

I have discovered that the warning appears as soon as in the Peripheral Signals of the Pins tool I enable OTG1_ID on pin GPIO_AD_09. The funny thing is that when I rout  pin OTG1_ID on pin GPIO_AD_09, the LPADC1 peripheral generate the warning for every conversion command that involve the B part of the ADC. (e.g. Channel sample mode = Single end mode, using B and Channel number=B, 1_0 » [T17] USB_OTG2_PWR/WL_DEV_WAKE/U354[10]/J10[2] or B, 1_2 » [P16] USB_OTG1_OC/U26[A2]/J26[4] or B, 1_3 » [L12] SPDIF_SR_CLK/ANATOP_32K_OUT/J26[8] etc....

I'm starting to think there is a bug in this part of the tool. The generated code per the pin mux looks correct to me (see below).

What's your opinion?

 

Kind regards,

Massimo

void BOARD_InitPins(void) {
CLOCK_EnableClock(kCLOCK_Iomuxc); /* LPCG on: LPCG is ON. */

IOMUXC_SetPinMux(
IOMUXC_GPIO_AD_06_GPIO_MUX3_IO05, /* GPIO_AD_06 is configured as GPIO_MUX3_IO05 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_AD_07_GPIO_MUX3_IO06, /* GPIO_AD_07 is configured as GPIO_MUX3_IO06 */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_AD_09_USBPHY1_OTG_ID, /* GPIO_AD_09 is configured as USBPHY1_OTG_ID */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_AD_24_LPUART1_TXD, /* GPIO_AD_24 is configured as LPUART1_TXD */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
IOMUXC_GPIO_AD_25_LPUART1_RXD, /* GPIO_AD_25 is configured as LPUART1_RXD */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinConfig(
IOMUXC_GPIO_AD_24_LPUART1_TXD, /* GPIO_AD_24 PAD functional properties : */
0x02U); /* Slew Rate Field: Slow Slew Rate
Drive Strength Field: high drive strength
Pull / Keep Select Field: Pull Disable, Highz
Pull Up / Down Config. Field: Weak pull down
Open Drain Field: Disabled
Domain write protection: Both cores are allowed
Domain write protection lock: Neither of DWP bits is locked */
IOMUXC_SetPinConfig(
IOMUXC_GPIO_AD_25_LPUART1_RXD, /* GPIO_AD_25 PAD functional properties : */
0x02U); /* Slew Rate Field: Slow Slew Rate
Drive Strength Field: high drive strength
Pull / Keep Select Field: Pull Disable, Highz
Pull Up / Down Config. Field: Weak pull down
Open Drain Field: Disabled
Domain write protection: Both cores are allowed
Domain write protection lock: Neither of DWP bits is locked */
}

0 件の賞賛
返信
4,520件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @Max83 ,

Yes, it seems like a bug. I'll report it. You can ignore the warning message.

 

Regards,

Jing

0 件の賞賛
返信
4,516件の閲覧回数
Max83
Contributor II

Hi @jingpan ,

thank you for your reply. May you tell me where I can find chip related informations? For instance, is there any document that specify the pin couple that I have to use for a differential voltage conversion? I can't find this information in the reference manual.

Kind regards,

Massimo

0 件の賞賛
返信
4,507件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @Max83 ,

That is in datasheet.

https://www.nxp.com/docs/en/data-sheet/IMXRT1170CEC.pdf

 

Regards,

Jing

0 件の賞賛
返信