Keil SDK Error: RDDI-DAP Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Keil SDK Error: RDDI-DAP Error

11,136 Views
brli
Contributor III

Hi, 

Could you help to suggest the error: RDDI-DAP Error? 

Attached are setting captures.

Develop Environment:

Board : IMXRT1050-EVKB

SDK : Keil 5.24

Thanks!

Best regards!

Br Li

0 Kudos
Reply
3 Replies

10,164 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Thank you for your interest in NXP RT produt, I would like to provide serivce for you.

Please check your on board debugger, CMSIS DAP or others?

The on board IMXRT1050-EVKB debugger can support CMSIS DAP and JLINK.

You can find it from:Control Panel\Hardware and Sound\Devices and Printers\unspecified

If it is the DAPLINK CMSIS DAP, it means your on board debugger is CMSIS DAP, you need to chose the CMSIS DAP In the keil.

From your picture, your MDK didn't select the correct debugger interface.

Please refer to my picture choose the correct debugger.

 

Wish it helps you!

 

If you still have question about it, please kindly let me know.

 

Have a great day,

Kerry

 

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

 

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply

10,164 Views
brli
Contributor III

Hi Rita,

My debuger is on board CMSIS DAP, please refer attached capture.

The error is either "RDDI-DAP Error" or "SWD/JTAG Communication Failure" when changing Max Clock.

Have a great day!

Br Li

rt1050_debug_error.PNG

0 Kudos
Reply

10,164 Views
danielbujak
Contributor III

Was there any resolution to this?

0 Kudos
Reply