JPEG Image compression

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

JPEG Image compression

跳至解决方案
3,148 次查看
hitesh_gambhava
Contributor I

Hi,

In my application, I am using SPI camera module which is giving VGA (640x480) output in RGB or YUV format.

I want to compressed this image in JPEG format so I can send it over wireless easily. I read in i.MXRT1050 application note that this is possible. See following BD.

hitesh_gambhava_0-1697781461174.png

My question - Is this possible on i.MXRT1170 as well as both containts the PXP module for such conversion. Also, this is practical acheivable approach to do JPEG compression of the RGB or YUV image from some storage flash?

Thanks,

Hitesh

标记 (1)
0 项奖励
回复
1 解答
3,113 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

Yes, it is possible to use jpeg library to compress an image on RT1170. Please note that this process is made by the CPU and not the PXP module.
It is possible as well to use some flash for the image source(see sd_jpeg example). You only need to make sure that Flash is not used for XIP.

Best regards,
Omar

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,097 次查看
hitesh_gambhava
Contributor I

Thank you Omar for the response and confirmation.

0 项奖励
回复
3,114 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

Yes, it is possible to use jpeg library to compress an image on RT1170. Please note that this process is made by the CPU and not the PXP module.
It is possible as well to use some flash for the image source(see sd_jpeg example). You only need to make sure that Flash is not used for XIP.

Best regards,
Omar

0 项奖励
回复