Hello,
I am attempting to bring up the EVK-MIMXRT685 evaluation board. I am following the videos/instructions in the "Getting Started with i.MX RT600 Evaluation Kit" pages on the NXP site. I have successfully installed all of the necessary applications as per the instructions.
When I attempt to debug the SDK example (dsp_mu_pollng_cm33), I receive an error stating that the evkmimxrt685.JLinkScript file cannot be found by the debugger. The folder listed in the error message is empty.
The second error message received states that "No connection could be make because the target machine actively refused it."
After this initial connection failure, I deleted all applications and re-installed them again. However, I receive the same error messages when attempting to debug the program.
Screenshots of the errors are attached.
I am running the MCUXpresso IDE on a Windows 10 VMware virtual machine. I verified that the evaluation board is connected to the guest OS. Previously, I have run MCUXpresso on a Windows 10 VM with a FRDM-K64F evaluation board with no issues.
Can anyone provide an answer or point me in the right direction?
Thanks in advance for your help.