Issue running SDK example code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue running SDK example code

1,787件の閲覧回数
RMG
Contributor II

I have a MIMXRT1160-EVK. It seems that I can no longer run SDK sample code. I am not certain if I have downloaded something to the board that may have caused this issue; I may have tried to load a Linux variant incorrectly. I have tried to run the "evkmimxrt1160_iled_blinky_cm7" example, which I believe is what is on the CCA when delivered. The example will build, but will not run. The "Problem Occurred" details is pretty wordy, but says this:

Error starting process.
Cannot run program "C:\Users\xxx\Documents\MCUXpressoIDE_11.5.1_7266\workspace\evkmimxrt1160_iled_blinky_cm7\Debug\evkmimxrt1160_iled_blinky_cm7.axf": Launching failed
Cannot run program "C:\Users\xxx\Documents\MCUXpressoIDE_11.5.1_7266\workspace\evkmimxrt1160_iled_blinky_cm7\Debug\evkmimxrt1160_iled_blinky_cm7.axf": Launching failed
Cannot run program "C:\Users\xxx\Documents\MCUXpressoIDE_11.5.1_7266\workspace\evkmimxrt1160_iled_blinky_cm7\Debug\evkmimxrt1160_iled_blinky_cm7.axf": Launching failed

Is there any way to determine what happened here? Can I revert back to the configuration of a newly delivered EVK? I have not moved any jumpers of DIP switches.

0 件の賞賛
返信
2 返答(返信)

1,776件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

In order to understand I have some questions, Could you tell me if you are using the debugger on the boar or an external debugger? Could you share the state of the dipswitch? Could you share the state of the jumpers?

Best regards,
Pavel

0 件の賞賛
返信

1,769件の閲覧回数
RMG
Contributor II

Hello Pavel-

I have debug sessions working now. It was a simple issue of not getting the debug example software correctly downloaded to the board. Thank you for taking the time to respond to my issue.

 

Rob

0 件の賞賛
返信