Is there a function example for OTFAD encryption?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a function example for OTFAD encryption?

1,698件の閲覧回数
Vinos
Contributor III

if OTFAD is enabled,the firmware was encrypted using image_enc.exe on Windows, but now I want to encrypt some fields in the program.

I have seen the source code of image_enc on GitHub, but it takes up a lot of memory if placed the AES-related code in NOR Flash. 

Is there any code example that can encrypt plaintext into corresponding ciphertext based on the current OTFAD IEK in the RT1170 chip?

 

I've found relevant functions in https://mcuxpresso.nxp.com/api_doc/dev/2304/a00047.html,it seems SDK of other RT chips support OTFAD examples.RT1170 doesn't have relevant implementaions in the SDK?

0 件の賞賛
返信
1 返信

1,670件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信