Hi!
There is a custom PCB and custom application not related with vision or voice processing.
The PCB/application were designed for MIMXRT1176. But it is difficult to perchase this part, while MIMXRT117H parts are available.
-------------------------
could one solder MIMXRT117H instead of MIMXRT1176 on the board and run custom application on the CPU?
If yes:
will software develompent procedure and board bring up differ from regular procedure for MIMXRT1176 or not?
BR,
Sergey.
解決済! 解決策の投稿を見る。
You are welcome!
If your question is solved, please help to mark the correct answer, just to close this case, thanks.
Any new issues, welcome to create the new case.
Best Regards,
Kerry
Thank you!
You are welcome!
If your question is solved, please help to mark the correct answer, just to close this case, thanks.
Any new issues, welcome to create the new case.
Best Regards,
Kerry
Hi @sergio19 ,
Yes, you can use the RT117H to replace the RT1176.
But, please note, the RT117H is single core, not the dual core:
You can consider the RT117F is the RT1172, but RT117F can support the NXP’s EdgeReady MCU-based solution.
Wish it helps you!
Best Regards,
kerry
Thank you for information!
But from the table you attached and from the datasheet : MIMXRT117H is dual core, it has 1Gb Ethernet and other features similar to MIMXRT1176. Could you please repeat that HW of MIMXRT117H part defers from the HW of MIMXRT1176 (dual/single core, etc.)?
I am worried about EdgeReady sollution: does the software stack part located in the MCU affect compatibility with "bare metal" application written for MIMXRT1176?
BR,
Sergey.
Hi @sergio19 ,
Sorry, you mean RT117H, not RT117F.
Yes, RT117H is the same as RT1176, to the "bare metal" , it's totally OK.
Please note, RT117H have more function than RT1176, so, don't worry if just bare-metal.
Best Regards,
kerry