Is it possible to replace MIMXRT1176 by MIMXRT117H ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to replace MIMXRT1176 by MIMXRT117H ?

Jump to solution
1,004 Views
sergio19
Contributor I

Hi!

There is a custom PCB and custom application not related with vision or voice processing.

The PCB/application were designed for MIMXRT1176. But it is difficult to perchase this part, while MIMXRT117H  parts are available.

-------------------------

could one solder MIMXRT117H  instead of MIMXRT1176 on the board and run custom application on the CPU?

If yes:

will software develompent procedure and board bring up differ from regular procedure for MIMXRT1176 or not?

BR,

Sergey.

 

 

Tags (1)
0 Kudos
Reply
1 Solution
944 Views
kerryzhou
NXP TechSupport
NXP TechSupport

@sergio19 ,

  You are welcome!

  If your question is solved, please help to mark the correct answer, just to close this case, thanks.

Any new issues, welcome to create the new case.

Best Regards,

Kerry

View solution in original post

0 Kudos
Reply
5 Replies
962 Views
sergio19
Contributor I

Thank you!

0 Kudos
Reply
945 Views
kerryzhou
NXP TechSupport
NXP TechSupport

@sergio19 ,

  You are welcome!

  If your question is solved, please help to mark the correct answer, just to close this case, thanks.

Any new issues, welcome to create the new case.

Best Regards,

Kerry

0 Kudos
Reply
975 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sergio19 ,

  Yes, you can use the RT117H to replace the RT1176.

 But, please note, the RT117H is single core, not the dual core:

kerryzhou_0-1681707479712.pngkerryzhou_1-1681707485905.png

You can consider the RT117F is the RT1172, but RT117F can support the NXP’s EdgeReady MCU-based solution.

Wish it helps you!

Best Regards,

kerry

 

0 Kudos
Reply
968 Views
sergio19
Contributor I

Thank you for information!

But from the table you attached and from the datasheet : MIMXRT117H is dual core, it has 1Gb Ethernet and other features similar to MIMXRT1176. Could you please repeat that HW of MIMXRT117H part defers from the HW of MIMXRT1176 (dual/single core, etc.)?

I am worried about EdgeReady sollution: does the software stack part located in the MCU affect compatibility with "bare metal" application written for MIMXRT1176?

BR,

Sergey.

0 Kudos
Reply
966 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sergio19 ,

  Sorry, you mean RT117H, not RT117F.

  Yes, RT117H is the same as RT1176, to the "bare metal" , it's totally OK.

  Please note, RT117H have more function than RT1176, so, don't worry if just bare-metal.

 

Best Regards,

kerry

0 Kudos
Reply