Inline encryption engine(IEE) for External flash memory in IMXRT1170

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inline encryption engine(IEE) for External flash memory in IMXRT1170

Jump to solution
3,597 Views
Nagaveni
Contributor II

Hi, 

I am using IMXRT1170 Evk ,

  1. can I use IEE(Inline encryption engine) for both encryption and decryption to   read and write to the external flash memory ?
  2. please find below image  and can you tell us what is difference between 8.1.2 section from security RM manual and 7.10 section from IMXRT1170RM manual ?

  

Nagaveni_0-1678529927799.png

 

Nagaveni_1-1678529987132.png

Thanks in advance

 

 

0 Kudos
Reply
1 Solution
3,527 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Thank you for your patience!
The IEE features on the SRM don't take the system limitations of RT1170. So IEE on RT1170 can only decrypt FlexSPI Nor memory.

Best regards,
Omar

View solution in original post

0 Kudos
Reply
3 Replies
3,555 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

IEE on flexspi is only capable of decryption, however, let me confirm if it is also possible to encrypt flexspi through IEE.

Best regards,
Omar

0 Kudos
Reply
3,546 Views
Nagaveni
Contributor II

Thank you for the response,

Please confirm ASAP, Regarding IEE encryption for Flash memory

0 Kudos
Reply
3,528 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Thank you for your patience!
The IEE features on the SRM don't take the system limitations of RT1170. So IEE on RT1170 can only decrypt FlexSPI Nor memory.

Best regards,
Omar

0 Kudos
Reply