IMXRT1064 Firmware Update

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXRT1064 Firmware Update

1,326件の閲覧回数
sagar_prajapati
Contributor II

Hello all,

I am trying to update firmware using ISP mode on IMXRT1064 using boot ROM. I want to know, Is there a software/programmatic method to enable ISP at System Reset without using switches?  So many people asking for this solution. Please provide document or working example for this.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,200件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Sagar Prajapati,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
In the RT1064, the ROM APIs provide an API to re-enter serial downloader mode for image update, I think it can implement your application.

pastedImage_24.png

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信