IMXRT1052 SW7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1052 SW7

Jump to solution
2,256 Views
vwsncr
Contributor II

 

Must the pin connected to the four switches in the picture be set to the default value?

Example , if i use QSPIFLASH , i need set 0010?

 

 

sw7.jpg

Labels (1)
0 Kudos
Reply
1 Solution
2,250 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
In my opinion, I'd like to suggest you go through the Chapter 9 System Boot of RT1052's RM to have an overview of the boot mode of the RT MCU, then you'll how to configure boot pins to boot from the QSPI flash
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

1 Reply
2,251 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
In my opinion, I'd like to suggest you go through the Chapter 9 System Boot of RT1052's RM to have an overview of the boot mode of the RT MCU, then you'll how to configure boot pins to boot from the QSPI flash
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------