IMXRT1024 CCM Clock Observability Output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1024 CCM Clock Observability Output

Jump to solution
2,811 Views
Lukas_Frank
Senior Contributor I

Hi all,

 

I am on my project to do configurations of clock connections. I did not fully understand function of CCM_CLKO1 and CCM_CLKO2 signals. 

Reference Manual says :

14.2.1 Features

Selects clock signals to output on CCM_CLKO onto the pads for observability.

What observability means us here? For example I have two active clock that I used in my system (i.e. GPT and QTMR) at the same time. What kind of things will I observe from these CCM signals (CCM_CLKO1 and CCM_CLKO2)

 

Thanks and Regards.

0 Kudos
Reply
1 Solution
2,798 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
Q1: What if there is not a Clock Observability Output? So, what is the advantages of it? What kind of parameters is exist that we can observe from an oscilloscope?
-- After mentioned above, we can select some clock sources to output via the CCM_CLKO1 and CCM_CLKO2 pins, then use the oscilloscope to observe them check their frequency is the expected value.
Q2: Which document and program did you use to see that figure?
Hope it helps.
-- The above figure is the screenshot of the MCUXpresso Config Tools which provides a graphical representation of the MCU clock tree system and interactive user controls as well as assistance with system fine-tuning.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,805 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)What observability means us here? For example I have two active clock that I used in my system (i.e. GPT and QTMR) at the same time. What kind of things will I observe from these CCM signals (CCM_CLKO1 and CCM_CLKO2)
-- Just as the below figure shows, we can select some clock sources to output via the CCM_CLKO1 and CCM_CLKO2 pins, then use the oscilloscope to observe them.

jeremyzhou_0-1625110440384.png

Hope it helps.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,802 Views
Lukas_Frank
Senior Contributor I

Hi Dear @jeremyzhou ,

 

Q1: What if there is not a Clock Observability Output? So, what is the advantages of it? What kind of parameters are exist that we can observe from oscilloscope?

Q2: Which document and program did you use to see that figure?

 

Thanks and Regards.

0 Kudos
Reply
2,799 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
Q1: What if there is not a Clock Observability Output? So, what is the advantages of it? What kind of parameters is exist that we can observe from an oscilloscope?
-- After mentioned above, we can select some clock sources to output via the CCM_CLKO1 and CCM_CLKO2 pins, then use the oscilloscope to observe them check their frequency is the expected value.
Q2: Which document and program did you use to see that figure?
Hope it helps.
-- The above figure is the screenshot of the MCUXpresso Config Tools which provides a graphical representation of the MCU clock tree system and interactive user controls as well as assistance with system fine-tuning.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply