IMXRT1010 LPI2C problem using debug mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1010 LPI2C problem using debug mode

Jump to solution
1,269 Views
LuigiV
Contributor III

I use the IMXRT1010 EVK and the MCUXpresso; I configured the LPI2C in transfer mode and the SAI in interrupt mode (word); both units work right but not at the same time.

The LPI2C works correctly only when I don't enable the SAI interrupt, if I enable the SAI interrupt the

"LPI2C_MasterWaitForTxReadyF(LPI2Cbase)" seems to freeze the code....

Anyone may help me ?

Thank you, Luigi

 

 

0 Kudos
Reply
1 Solution
1,244 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

Could you please tell me the SDK version you are using?
Could you confirm SAI works correctly if it runs independently?
By debug mode you mean you have a debug session running, am I right? Is this problem still occurs if you don't run it with the debug session?

Regards,
Daniel.

View solution in original post

0 Kudos
Reply
2 Replies
1,245 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

Could you please tell me the SDK version you are using?
Could you confirm SAI works correctly if it runs independently?
By debug mode you mean you have a debug session running, am I right? Is this problem still occurs if you don't run it with the debug session?

Regards,
Daniel.

0 Kudos
Reply
1,222 Views
LuigiV
Contributor III
Hi Daniel,
I apologize I haven't signed the post as "solved"...

Thanks anyway, Luigi
0 Kudos
Reply