IMXRT quad timers synchronization

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMXRT quad timers synchronization

跳至解决方案
2,236 次查看
dinartal
Contributor III

Is it possible to synchronize two quad timers to get 64bit timer with 8 capture inputs?

标签 (2)
0 项奖励
回复
1 解答
2,209 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Can we sync them together?
-- No, I'm afraid that they (two 64 bit quad timers) can't be synced.
I've answered your question in another post, please check it.
Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
2,225 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)Is it possible to synchronize two quad timers to get 64bit timer with 8 capture inputs?
-- Actually, I'm not very clear with your question, so I was wondering if you can explain it again.
Looking forward to your reply.
Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
2,214 次查看
dinartal
Contributor III

Let me try to explain my question: in IMXRT1020 we have two 64 bit quad timers TMR0 & TMR1 (4x16 cascaded). can we sync them together? it means that at any time there are same values in count registers. Count registers of both timers increase(decrese) simultinously.

0 项奖励
回复
2,210 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Can we sync them together?
-- No, I'm afraid that they (two 64 bit quad timers) can't be synced.
I've answered your question in another post, please check it.
Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------