IMXRT - Azure GUIX Screen issues : Overlay, Color inversion, Freeze

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT - Azure GUIX Screen issues : Overlay, Color inversion, Freeze

1,114 Views
Ric
Contributor I

Hi, NXP community, 

I encounter 3 issues using Azure GUIX on IMXRT1062 target. I am using a New Haven display: NHD-4.3-HDMI-HR-RSXP

The issues are the following :

  • Image Overlay: After a certain period of time, texts and images start remaining on-screen even after being detached using gx_widget_detach() and after switching off/on the system.
  • Color inversion: To illustrate this issue, on GUIX Studio I have a green box, but when the program is loaded on target, the screen returns a red box. I am on a 24 bits project in GUIX Studio and my MCU project also. I use an XRGB888 pixel format for the display
  • Screen Freeze : At some point, when the screen is running, some times the actual screen freezes, and trying to change the screen to set another one has no effect

I want to know if there are some parameters to configure in order to solve this, and what are they or other solutions.

I join to this request some images of the init process.

Thanks to you all

Ric_0-1686910338125.png

Ric_1-1686910387677.pngRic_2-1686910400131.pngRic_3-1686910419651.png

 

Ric_12-1686917466204.png

Ric_6-1686910533219.png

Ric_7-1686910545911.pngRic_8-1686910558471.png

 

 

Ric_9-1686910676737.pngRic_10-1686910684151.png

0 Kudos
Reply
0 Replies