IMX Rt 1176 M4 Master M7 Slave Project Example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX Rt 1176 M4 Master M7 Slave Project Example

Jump to solution
2,728 Views
tbayram
Contributor IV

Hello Everyone,

İs there any example for M4 master M7 slave project for IMX RT1176.

 

Thank you.

0 Kudos
Reply
1 Solution
2,710 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

In the i.MX RT1170 page you can find the app note AN13574 with its respective associated SW file.

_Leo__0-1710181154923.png

Hope it helps you.

Have a nice day!

View solution in original post

0 Kudos
Reply
3 Replies
2,706 Views
tbayram
Contributor IV

thanks @_Leo_ .

 

0 Kudos
Reply
2,703 Views
tbayram
Contributor IV

Hi @_Leo_,
İs there any different way to make this?
Because of there is no usb connection on our custom board.

I am using the application board commands on EVK board but, I think blhost is not working properly. Because I couldnt see "This is the init image to setup CM4 primary core environment. " information on the console. some step on the program.bat couldn't be success. And when I try to upload SDK (M4 master M7 slave). give me error to upload.

Thank for helping

0 Kudos
Reply
2,711 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

In the i.MX RT1170 page you can find the app note AN13574 with its respective associated SW file.

_Leo__0-1710181154923.png

Hope it helps you.

Have a nice day!

0 Kudos
Reply