IMX Rt 1176 M4 Master M7 Slave Project Example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX Rt 1176 M4 Master M7 Slave Project Example

ソリューションへジャンプ
2,684件の閲覧回数
tbayram
Contributor IV

Hello Everyone,

İs there any example for M4 master M7 slave project for IMX RT1176.

 

Thank you.

0 件の賞賛
返信
1 解決策
2,666件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

In the i.MX RT1170 page you can find the app note AN13574 with its respective associated SW file.

_Leo__0-1710181154923.png_Leo__0-1710181154923.png

Hope it helps you.

Have a nice day!

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,662件の閲覧回数
tbayram
Contributor IV

thanks @_Leo_ .

 

0 件の賞賛
返信
2,659件の閲覧回数
tbayram
Contributor IV

Hi @_Leo_,
İs there any different way to make this?
Because of there is no usb connection on our custom board.

I am using the application board commands on EVK board but, I think blhost is not working properly. Because I couldnt see "This is the init image to setup CM4 primary core environment. " information on the console. some step on the program.bat couldn't be success. And when I try to upload SDK (M4 master M7 slave). give me error to upload.

Thank for helping

0 件の賞賛
返信
2,667件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

In the i.MX RT1170 page you can find the app note AN13574 with its respective associated SW file.

_Leo__0-1710181154923.png_Leo__0-1710181154923.png

Hope it helps you.

Have a nice day!

0 件の賞賛
返信