IMX RT1020 CEC external flash programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX RT1020 CEC external flash programming

2,939 Views
b_iouri
Contributor I

Hello,

we have custom design based on IMXRT 1020 development board. CPU IMXRT1020 CEC, serial flash IS25LP064.

Boot strap configuration: A0 - A12 (except A10) has 47 K pull down resistors; A1 also has 1K pull up resistor.

Using JLINK to program the flash...

During the programming we can probe and see activities on follow SPI lines: CS/SO/SI/SCK. Issue what we are having once programming is complete and IMX RT suppose to boot up, we do see activities on SCK and CS, but nothing coming from SO (line from Serial Flash to MCU).

Any word of advise...

Thank you.

Labels (1)
0 Kudos
Reply
3 Replies

2,711 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi i b ,

  Please use the JLINK commander to check your customer board with the SWD interface, whether you can find the ARM core or not?

  If you can find the ARM core, please configure the BOOT_CFG[1]-BOOT_CFG[6] to 0, BOOT_CFG2[0]-[1] to 0, BOOT mode configure to the serial download mode, you can find the related BOOT-CFG and BOOT_MODE pins in this table:

pastedImage_1.png

pastedImage_2.png

then use the MCUBootUtility to connect your board and download the code to the QSPI flash.

Please try it at first.

If you still have questions about it, please kindly let us know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,711 Views
jay_heng
NXP Employee
NXP Employee

MCUBootUtility tool is fully verified on RT1020

0 Kudos
Reply

2,711 Views
jay_heng
NXP Employee
NXP Employee
0 Kudos
Reply