I am looking to buy Ulink2 programmer?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I am looking to buy Ulink2 programmer?

1,142 次查看
sanketkulkarni
Contributor III

I am looking to buy Ulink2 Programmer of ARM, the question comes to mind will it work on most of the boards? I want to a debugger which is universal and can work with any board. Ulink2 is in my bugdet, so I am asking this question. I am also looking for Segger Jlink as a universal debugger. Or there is another option in these regard?  

   Also, will Ulink2 will work i.mx 1020 board?

标记 (1)
0 项奖励
回复
1 回复

1,099 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Sanket kulkarni

According to the Keil page, ULINK2 supports:

pastedImage_1.png

as long as the RT1020 is a Cortex M7, it does support this chip. you can find more information in their web page:

ULINK Debug Adapters 

Hope this information helps.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 项奖励
回复