I.MX RT1024 POR_B pin is not used

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX RT1024 POR_B pin is not used

Jump to solution
3,672 Views
Rajender
Contributor I

Hi,

I am designing a custom board using i.mx RT1024 MCU.

In the EVK the POR_B signal is driven with a reset supervisor IC but in our schematic we would like to not use external POR as internal POR does the same function.

Are there any other issues i may face if i don't external POR? or is it normal to not use external POR?

 

0 Kudos
Reply
1 Solution
3,662 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Are there any other issues i may face if i don't external POR? or is it normal to not use external POR?
-- -To be prudent, I'd like to know the exact meaning of not using the external POR.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
3,663 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Are there any other issues i may face if i don't external POR? or is it normal to not use external POR?
-- -To be prudent, I'd like to know the exact meaning of not using the external POR.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
3,659 Views
Rajender
Contributor I

Hi jeremy,

Thanks for your quick reply!

By mentioning external POR, i was referring to POR_B pin of the MCU which is AND'ed with internal POR of MCU. It is mentioned that if POR_B is not used then it can be unconnected or pull high but i want to know will there by any other issues during bootup/power up if POR_B left unconnected.

 

Regards,

Rajender

Rajender_0-1653898742934.png

 

0 Kudos
Reply
3,649 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
There are some issues that may arise, such as boot-up instability, can't use boot_mode pins to configure the boot mode, etc.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

 

0 Kudos
Reply
3,646 Views
Rajender
Contributor I

Hi Jeremy,

I didn't get it! Can you please elaborate more on it? or can you please share any documentation related to it?

 

Rajender_0-1653986768593.png

 

This is how i unconnected POR_B in the schematic.

 

Regards,

Rajender.

0 Kudos
Reply
3,636 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Can you please elaborate more on it? or can you please share any documentation related to it?
-- As the Hardware Development Guide for the
MIMXRT1050/MIMXRT1060 Processor, the i.MX RT needs to follow the sequence of the below power-up, further, the BOOT_MODE register is initialized by sampling the BOOT_MODE0 and
BOOT_MODE 1 inputs on the rising edge of the POR_B, to make sure the system boot with stability, it's usually recommended to use an external reset IC to connect the POR_B in the design actually.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply