How to make a file can store more than 512 bytes with FileX_LevelX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to make a file can store more than 512 bytes with FileX_LevelX

2,350 Views
BryceHuang
Contributor I

I used FileX & Level_X
The nor-flash is 128MBit  the sector size is 4096 bytes.
But I found I only can save 512 bytes of data per file.
I read nor-flash by the nor-flash programmer.
The data over 512 bytes are lost.
Does anyone know the correct method to let fx_file_write can write the data over 512 bytes or 1K 2K~1M
into one file?



0 Kudos
Reply
3 Replies

2,338 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @BryceHuang 

I hope you are doing well. 

Could you please let me know  your  specific MCU? 

Best regards, 

Diego

0 Kudos
Reply

2,289 Views
BryceHuang
Contributor I

@diego_charles 
My MCU is LPC55S69.

0 Kudos
Reply

2,125 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @BryceHuang 

I just wanted to make a follow up on this. 

Basically The the file size should be determined by the size of the buffer given to  fx_file_write 

diego_charles_0-1693612116419.png

And also the file size  can increase thanks to the fx_file_seek, 

Below and output example where I use a 1K byte file.

 

FILEX example.....
Open RAM Disk.....
Create TEST.TXT.....
Write TEST.TXT.....

Recovered text file is:

FileX supports an unlimited number of media devices at the same time, including RAM disks, FLASH managers, and actual physical devices. It supports 12-, 16-, and 32-bit File Allocation Table (FAT) formats, and also supports Extended File Allocation Table (exFAT), contiguous file allocation, and is highly optimized for both size and performance. FileX also includes fault tolerant support, media open/close, and file write callback functions.Designed to meet the growing need for FLASH devices, FileX uses the same design and coding methods as ThreadX. Like all Azure RTOS products,FileX is distributed with full ANSI FileX provides the very best deeply embedded filesystem technology in a manner that is easy to understand and easy to use! The FileX Application Programming Interface (API) makes the services intuitive and consistent. You won't have to decipher

Close TEST.TXT.....

 

If this issue persisted, please share any changes you have made to the filex_levelx_spiflash example. As well return errors you saw from the filex APIs.

In the case you need to adapt further the driver for your memory, I would suggest to start with ramdisk version for the demo, this version does not use Level X, as RAM does not wear like flash. Set DEMO_SECTOR and DEMO_DISK parameters accoriding your flash memory. The advantage of this that RAM does not have the sector size constrains that flash have.  I use the ramdisk demo as a base to diagnose issues and determine if the errrors are located within the flash driver itself.

Best regards, 

Diego

 

Also SDK 2.14.0 for the LPC55s69 is already there so you may try this latest SDK

 

0 Kudos
Reply