How to connect two codecs to a IMXRT processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to connect two codecs to a IMXRT processor

Jump to solution
1,129 Views
LuigiV
Contributor III

Hi,

I have to connect a four channels codec (AK4619) to a IMXRT processor, for example the IMXrt1011 (I have the evaluation board) or the IMXrt1021...IMXrt1062..., or two codecs to a IMXRT processor.

May you help me how to do it and if does exist a code example ?

 

Thank you.

 

Luigi 

0 Kudos
Reply
1 Solution
1,104 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Please refer to this example to use the multichannel feature of the SAI module: Using Multi-Channel Feature of SAI (nxp.com)
From RT1020 SAI1 supports up to 8 channels.

Best regards,
Omar

View solution in original post

0 Kudos
Reply
1 Reply
1,105 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Please refer to this example to use the multichannel feature of the SAI module: Using Multi-Channel Feature of SAI (nxp.com)
From RT1020 SAI1 supports up to 8 channels.

Best regards,
Omar

0 Kudos
Reply