How to connect two codecs to a IMXRT processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to connect two codecs to a IMXRT processor

ソリューションへジャンプ
1,182件の閲覧回数
LuigiV
Contributor III

Hi,

I have to connect a four channels codec (AK4619) to a IMXRT processor, for example the IMXrt1011 (I have the evaluation board) or the IMXrt1021...IMXrt1062..., or two codecs to a IMXRT processor.

May you help me how to do it and if does exist a code example ?

 

Thank you.

 

Luigi 

0 件の賞賛
返信
1 解決策
1,157件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Please refer to this example to use the multichannel feature of the SAI module: Using Multi-Channel Feature of SAI (nxp.com)
From RT1020 SAI1 supports up to 8 channels.

Best regards,
Omar

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,158件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Please refer to this example to use the multichannel feature of the SAI module: Using Multi-Channel Feature of SAI (nxp.com)
From RT1020 SAI1 supports up to 8 channels.

Best regards,
Omar

0 件の賞賛
返信