How does core clock affect uboot/kernel?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How does core clock affect uboot/kernel?

1,590件の閲覧回数
alain_olivier
Contributor I

Hello,

I plan to use IMXRT1021 for a project, but I notice the industrial and customer versions have a different core clock, 400 MHz and 500 MHz respectively. Is switching from one to the other something transparent or does it require uboot/kernel adjustments?

Thanks,

Alain.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,522件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Alain Olivier

The difference between the Industrial and the Consumer is the temperature range, level of accuracy with the voltage, freq, etc. So this is why the Frequency change between that datasheet. Since the image for uboot is chip specific, there should not change anything on this, but the uboot image should consider what chip would use.

Regards

Jorge Alcala

0 件の賞賛
返信