How does core clock affect uboot/kernel?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How does core clock affect uboot/kernel?

1,594 Views
alain_olivier
Contributor I

Hello,

I plan to use IMXRT1021 for a project, but I notice the industrial and customer versions have a different core clock, 400 MHz and 500 MHz respectively. Is switching from one to the other something transparent or does it require uboot/kernel adjustments?

Thanks,

Alain.

Labels (1)
0 Kudos
Reply
1 Reply

1,526 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Alain Olivier

The difference between the Industrial and the Consumer is the temperature range, level of accuracy with the voltage, freq, etc. So this is why the Frequency change between that datasheet. Since the image for uboot is chip specific, there should not change anything on this, but the uboot image should consider what chip would use.

Regards

Jorge Alcala

0 Kudos
Reply