Has anyone used vcnl4040 with any nxp microcontroller?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Has anyone used vcnl4040 with any nxp microcontroller?

1,004 Views
Jimmywder03
Contributor III

Hello,

 

I'm trying to used the vcnl4040 proximity sensor with Rt1052.

The vcnl4040 connect to my rt105

The problem is that I'm trying to implement the same the library that it was used (Arduino) to my rt1052.

I see how Arduino does something and then I try to to do the same in my Rt1052.

 

Is someone else can help me with that , will be fine.

 

Thanks for all 

 

0 Kudos
Reply
2 Replies

985 Views
Jimmywder03
Contributor III

Yes, im working on it but if anyone has worked with that sensor library, this will help me a  lot.

 

0 Kudos
Reply

988 Views
jay_heng
NXP Employee
NXP Employee

You might be the first one to port vcnl4040 library to i.mxrt.

Will be great if you can share your code when you done it.

0 Kudos
Reply