FreeRTOS Debugging in VS Code on RT1180-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeRTOS Debugging in VS Code on RT1180-EVK

1,079 Views
yanyanwang
Contributor I

In the evkmimxrt1180_freertos_message_buffers_secondary_core example project, the FreeRTOS configuration is as follows:

#define configMAX_PRIORITIES 56
#define configUSE_PORT_OPTIMISED_TASK_SELECTION 0
The application can be debugged normally in the IDE (MCUXpresso IDE). However, when debugging with VS Code, the debugger exits after FreeRTOS starts the scheduler.

The debug session terminates when execution reaches the following code in vTaskStartScheduler():

xNextTaskUnblockTime = portMAX_DELAY;
xSchedulerRunning = pdTRUE;
xTickCount = ( TickType_t ) configINITIAL_TICK_COUNT;
After these variables are initialized and before the first task is scheduled, the debugger disconnects and the debug session ends.

Could you help me test this in the IDE and VS Code and find a solution?

Labels (1)
0 Kudos
Reply
3 Replies

877 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi @yanyanwang,

After building the project in the Domains folder, you should find both the primary core and secondary core applications in this folder.

Pablo_Ramos_0-1782344180522.png

If you click the play button for both .elf files, does a debug session start for each of them?

If you run the primary core until it passes the MCMGR_StartCore function, are you able to pause the secondary core debug session?

Best Regards,
Pablo

0 Kudos
Reply

809 Views
yanyanwang
Contributor I

Hi,

 

I can successfully start a debug session on the secondary core, and everything works as expected before the FreeRTOS scheduler starts.

 

However, as soon as FreeRTOS starts scheduling tasks (after vTaskStartScheduler() is called), the debugger immediately disconnects and the debug session exits.

 

Could you please help me identify the possible cause of this issue? If there are any recommended debugger settings or FreeRTOS configurations that I should check, please let me know.

 

Thank you.

 

Best regards,

yanyan

0 Kudos
Reply

670 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi

Could you help me with the following questions?

How did you import the project?

Did you change any settings in the project?

Are you using an external debugger?

Best Regards,
Pablo

0 Kudos
Reply