Hi @gavin5342 ,
To the SDK FCB, it will all copied to the FlexSPI LUT with the ROM.
You can use the SDK example:
const flexspi_nor_config_t
hyperflash_config =
{
.memConfig =
{
.tag = FLEXSPI_CFG_BLK_TAG,
.version = FLEXSPI_CFG_BLK_VERSION,
.readSampleClksrc=kFlexSPIReadSampleClk_ExternalInputFromDqsPad,
.csHoldTime = 3u,
.csSetupTime = 3u,
.columnAddressWidth = 3u,
// Enable DDR mode, Wordaddassable, Safe configuration, Differential clock
.controllerMiscOption =
(1u << kFlexSpiMiscOffset_DdrModeEnable) | (1u << kFlexSpiMiscOffset_WordAddressableEnable) |
(1u << kFlexSpiMiscOffset_SafeConfigFreqEnable) | (1u << kFlexSpiMiscOffset_DiffClkEnable),
.deviceType = kFlexSpiDeviceType_SerialNOR,
.sflashPadType = kSerialFlash_8Pads,
.serialClkFreq = kFlexSpiSerialClk_133MHz,
.lutCustomSeqEnable = 0x1,
.sflashA1Size = 64u * 1024u * 1024u,
.dataValidTime = {15u, 0u},
.busyOffset = 15u,
.busyBitPolarity = 1u,
.lookupTable =
{
// Read LUTs
[0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0xA0, RADDR_DDR, FLEXSPI_8PAD, 0x18),
[1] = FLEXSPI_LUT_SEQ(CADDR_DDR, FLEXSPI_8PAD, 0x10, DUMMY_DDR, FLEXSPI_8PAD, 0x0C),
[2] = FLEXSPI_LUT_SEQ(READ_DDR, FLEXSPI_8PAD, 0x04, STOP, FLEXSPI_1PAD, 0x0),
// Read Status LUTs
// 0
[4 * 1 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
[4 * 1 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
[4 * 1 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
[4 * 1 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x70),
// 1
[4 * 2 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0xA0, RADDR_DDR, FLEXSPI_8PAD, 0x18),
[4 * 2 + 1] =
FLEXSPI_LUT_SEQ(CADDR_DDR, FLEXSPI_8PAD, 0x10, DUMMY_RWDS_DDR, FLEXSPI_8PAD, 0x0B),
[4 * 2 + 2] = FLEXSPI_LUT_SEQ(READ_DDR, FLEXSPI_8PAD, 0x4, STOP, FLEXSPI_1PAD, 0x0),
// Write Enable LUTs
// 0
[4 * 3 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
[4 * 3 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
[4 * 3 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
[4 * 3 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
// 1
[4 * 4 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
[4 * 4 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x55),
[4 * 4 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x02),
[4 * 4 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x55),
// Erase Sector LUTs
// 0
[4 * 5 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
[4 * 5 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
[4 * 5 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
[4 * 5 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x80),
// 1
[4 * 6 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
[4 * 6 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
[4 * 6 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
[4 * 6 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
// 2
[4 * 7 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
[4 * 7 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x55),
[4 * 7 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x02),
[4 * 7 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x55),
// 3
[4 * 8 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, RADDR_DDR, FLEXSPI_8PAD, 0x18),
[4 * 8 + 1] = FLEXSPI_LUT_SEQ(CADDR_DDR, FLEXSPI_8PAD, 0x10, CMD_DDR, FLEXSPI_8PAD, 0x0),
[4 * 8 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x30, STOP, FLEXSPI_1PAD, 0x0),
// Page Program LUTs
// 0
[4 * 9 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
[4 * 9 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
[4 * 9 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
[4 * 9 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xA0),
// 1
[4 * 10 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, RADDR_DDR, FLEXSPI_8PAD, 0x18),
[4 * 10 + 1] =
FLEXSPI_LUT_SEQ(CADDR_DDR, FLEXSPI_8PAD, 0x10, WRITE_DDR, FLEXSPI_8PAD, 0x80),
// Erase Chip LUTs
// 0
[4 * 11 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
[4 * 11 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
[4 * 11 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
[4 * 11 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x80),
// 1
[4 * 12 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
[4 * 12 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
[4 * 12 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
[4 * 12 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
// 2
[4 * 13 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
[4 * 13 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x55),
[4 * 13 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x02),
[4 * 13 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x55),
// 3
[4 * 14 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
[4 * 14 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
[4 * 14 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
[4 * 14 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x10),
},
// LUT customized sequence
.lutCustomSeq = {{
.seqNum = 0,
.seqId = 0,
.reserved = 0,
},
{
.seqNum = 2,
.seqId = 1,
.reserved = 0,
},
{
.seqNum = 2,
.seqId = 3,
.reserved = 0,
},
{
.seqNum = 4,
.seqId = 5,
.reserved = 0,
},
{
.seqNum = 2,
.seqId = 9,
.reserved = 0,
},
{
.seqNum = 4,
.seqId = 11,
.reserved = 0,
}},
},
.pageSize = 512u,
.sectorSize = 256u * 1024u,
.ipcmdSerialClkFreq = 1u,
.serialNorType = 1u,
.blockSize = 256u * 1024u,
.isUniformBlockSize = true,
};
Best Regards,
Kerry