Flash & Debug Using Segger J-Link in RT1062 Custom Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flash & Debug Using Segger J-Link in RT1062 Custom Board

2,098 次查看
AnilRathod
Contributor II

Hello NXP Team,

IDE used: MCUXpresso IDE v11.8.1

SDK version : 2.14.1

Currently I am developing my Code into Teensy 4.0 Board. which based on i.MXRT 1062  (MIMXRT1062DVL6B). 

Now i will move onto custom board, So using SWD interface JLINK V9 Debugger Is it possible to directly flash .hex file using SEGGER J-Flash application can you verified ?

Also Using this V9 JLINK is it possible for debugging in MCUXpresso IDE?

 

标签 (1)
0 项奖励
回复
2 回复数

2,061 次查看
AnilRathod
Contributor II

Ok, Thank you very much

0 项奖励
回复

2,073 次查看
MultipleMonomials
Contributor IV

Yes!  You can use the J-Link Commander LoadFile command to flash a hex file onto the chip.  And MCUXpresso IDE does support the use of a J-Link probe.

0 项奖励
回复