Flash & Debug Using Segger J-Link in RT1062 Custom Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash & Debug Using Segger J-Link in RT1062 Custom Board

2,065 Views
AnilRathod
Contributor II

Hello NXP Team,

IDE used: MCUXpresso IDE v11.8.1

SDK version : 2.14.1

Currently I am developing my Code into Teensy 4.0 Board. which based on i.MXRT 1062  (MIMXRT1062DVL6B). 

Now i will move onto custom board, So using SWD interface JLINK V9 Debugger Is it possible to directly flash .hex file using SEGGER J-Flash application can you verified ?

Also Using this V9 JLINK is it possible for debugging in MCUXpresso IDE?

 

Labels (1)
0 Kudos
Reply
2 Replies

2,028 Views
AnilRathod
Contributor II

Ok, Thank you very much

0 Kudos
Reply

2,040 Views
MultipleMonomials
Contributor IV

Yes!  You can use the J-Link Commander LoadFile command to flash a hex file onto the chip.  And MCUXpresso IDE does support the use of a J-Link probe.

0 Kudos
Reply