Hello NXP Team,
IDE used: MCUXpresso IDE v11.8.1
SDK version : 2.14.1
Currently I am developing my Code into Teensy 4.0 Board. which based on i.MXRT 1062 (MIMXRT1062DVL6B).
Now i will move onto custom board, So using SWD interface JLINK V9 Debugger Is it possible to directly flash .hex file using SEGGER J-Flash application can you verified ?
Also Using this V9 JLINK is it possible for debugging in MCUXpresso IDE?
Yes! You can use the J-Link Commander LoadFile command to flash a hex file onto the chip. And MCUXpresso IDE does support the use of a J-Link probe.