Flash & Debug Using Segger J-Link in RT1062 Custom Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash & Debug Using Segger J-Link in RT1062 Custom Board

3,815件の閲覧回数
AnilRathod
Contributor II

Hello NXP Team,

IDE used: MCUXpresso IDE v11.8.1

SDK version : 2.14.1

Currently I am developing my Code into Teensy 4.0 Board. which based on i.MXRT 1062  (MIMXRT1062DVL6B). 

Now i will move onto custom board, So using SWD interface JLINK V9 Debugger Is it possible to directly flash .hex file using SEGGER J-Flash application can you verified ?

Also Using this V9 JLINK is it possible for debugging in MCUXpresso IDE?

 

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

3,778件の閲覧回数
AnilRathod
Contributor II

Ok, Thank you very much

0 件の賞賛
返信

3,790件の閲覧回数
MultipleMonomials
Contributor IV

Yes!  You can use the J-Link Commander LoadFile command to flash a hex file onto the chip.  And MCUXpresso IDE does support the use of a J-Link probe.

0 件の賞賛
返信