FLEXSPI Bus Clock Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FLEXSPI Bus Clock Issue

Jump to solution
6,421 Views
mjpovi
Contributor III

Hi,

I'm using FLEXPI to connect to a NOR Flash device.  I'm clocking the FLEXSPI at 132 MHz and 99 MHz, depending on clock divider (3 or 4), being driven by PLL2_PFD2_CLK (see settings, below).

My issue is that while the chip select waveform appears "okay" the SCLK and data lines do not appear to be driven very well, and I've tried the 100 MHz, 150 MHz, and 200MHz and speeds and all the drive-strength settings without success.  The only way I am successfull using the FLEXPI is to reduce the FLEXSPI clock to 99 MHz or slower.

I don't think that the clock and data lines are being driven successfully, except maybe for the SS0/Chip Select.  Can you recommend some settings to try or might I have an issue with the external bus H/W ?

pim_mux

IOMUXC_SetPinMux(IOMUXC_GPIO_SD_B1_06_FLEXSPIA_SS0_B, 1U);
IOMUXC_SetPinMux(IOMUXC_GPIO_SD_B1_07_FLEXSPIA_SCLK, 1U);     
IOMUXC_SetPinMux(IOMUXC_GPIO_SD_B1_08_FLEXSPIA_DATA00, 1U);
IOMUXC_SetPinMux(IOMUXC_GPIO_SD_B1_09_FLEXSPIA_DATA01, 1U);
IOMUXC_SetPinMux(IOMUXC_GPIO_SD_B1_10_FLEXSPIA_DATA02, 1U);
IOMUXC_SetPinMux(IOMUXC_GPIO_SD_B1_11_FLEXSPIA_DATA03, 1U);

IOMUXC_SetPinConfig(IOMUXC_GPIO_SD_B1_06_FLEXSPIA_SS0_B, 0x10E1U);
IOMUXC_SetPinConfig(IOMUXC_GPIO_SD_B1_07_FLEXSPIA_SCLK, 0x10E1U);
IOMUXC_SetPinConfig(IOMUXC_GPIO_SD_B1_08_FLEXSPIA_DATA00, 0x10E1U);
IOMUXC_SetPinConfig(IOMUXC_GPIO_SD_B1_09_FLEXSPIA_DATA01, 0x10E1U);
IOMUXC_SetPinConfig(IOMUXC_GPIO_SD_B1_10_FLEXSPIA_DATA02, 0x10E1U);
IOMUXC_SetPinConfig(IOMUXC_GPIO_SD_B1_11_FLEXSPIA_DATA03, 0x10E1U);

///////////////////////////////////////////////////////////////////////////

/* Disable Flexspi clock gate. */
CLOCK_DisableClock(kCLOCK_FlexSpi);
/* Set FLEXSPI_PODF. */
CLOCK_SetDiv(kCLOCK_FlexspiDiv, 2);
/* Set Flexspi clock source. */
CLOCK_SetMux(kCLOCK_FlexspiMux, 2);

//////////////////////////////////////////////////////////////////////////////////

clock_config

/* Init System PLL. */

CLOCK_InitSysPll(&sysPllConfig_BOARD_BootClockRUN);
/* Init System pfd0. */
CLOCK_InitSysPfd(kCLOCK_Pfd0, 27);
/* Init System pfd1. */
CLOCK_InitSysPfd(kCLOCK_Pfd1, 16);
/* Init System pfd2. */
CLOCK_InitSysPfd(kCLOCK_Pfd2, 24);
/* Init System pfd3. */
CLOCK_InitSysPfd(kCLOCK_Pfd3, 16);

/////////////////////////////////////////////////////////////////////////////

 

Labels (1)
0 Kudos
Reply
1 Solution
6,412 Views
jeremyzhou
NXP Employee
NXP Employee

Hi @mjpovi ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest support, please follow the below advice to modify the hardware board and test.,
1) It is recommended to left FLEXSPI_A_DQS(GPIO_SD_B1_05)pin floating;
2) It is also recommend to pull-up QSPI flash
#S and HOLD pins to make sure QSPI Flash boot up stability.
3) Using the tool to contact the board.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

1 Reply
6,413 Views
jeremyzhou
NXP Employee
NXP Employee

Hi @mjpovi ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest support, please follow the below advice to modify the hardware board and test.,
1) It is recommended to left FLEXSPI_A_DQS(GPIO_SD_B1_05)pin floating;
2) It is also recommend to pull-up QSPI flash
#S and HOLD pins to make sure QSPI Flash boot up stability.
3) Using the tool to contact the board.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------