FLEXRAM Configuration code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FLEXRAM Configuration code

2,599 Views
gustavoparlanti
Contributor I

FlexRAM  Configuration 

Hi 

I'm having problem to configure the FlexRAM in MIMXRT1021DAF5A, based on AN12077

I want to setup the following configuration 

project Config.PNG

and in the startup file I initialize the flexram controller with the following code

StartupCode.PNG

the problem that I have is I obtain compiller error that I cannot trace 

Console Problems.PNG

Console Errors.PNG

I could not understand where is my error if any could help me it is appreciated 

Thanks.

Gustavo Parlanti

0 Kudos
Reply
2 Replies

2,377 Views
746399664
Contributor I

你无法使用DAP链接是由于系统早就跑死,芯片上锁,你可以改变boot 方式,并断电重启。让芯片不跑程序,然后就可以下载新的程序了,至于原因,是由于配置出错了

0 Kudos
Reply

2,377 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Gustavo Parlanti ,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I'd like to give a test on my site, whether you can share the demo project.
Looking forward to your reply.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply