Ethernet based camera interfacing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet based camera interfacing

1,306 Views
jagadeesh_11
Contributor I

Hi,

Can we interface the IP camera in RT1170  EVK via ethernet.

Please Guide us.

 

Regards,

Jagadeesh

0 Kudos
Reply
1 Reply

1,291 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Jagadeesh,

You should be able to receive the IP camera stream on the i.MXRT1170. There is not an example with the IP Camera implementation per se. However, the i.MXRT1170 SDK have some Ethernet and lwip examples, which may help as a starting point.

Regards,
Gustavo

0 Kudos
Reply