ETHERNET COMMUNICATION

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ETHERNET COMMUNICATION

2,181件の閲覧回数
achal
Contributor III

PLEAE TELL in this below example how the developed decided these phy address and mac address

achal_0-1686485445062.png

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,096件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @achal ,

What you marked in the screenshot is mac address. PHY address is defined in board.h

 

/*! @brief The ENET PHY address. */
#define BOARD_ENET0_PHY_ADDRESS (0x02U) /* Phy address of enet port 0. */

 

 

Regards,

Jing 

0 件の賞賛
返信

2,004件の閲覧回数
achal
Contributor III

Hi @jingpan 

Thanks for responding, can you please tell why phy address is defined as  0x02 only and why not something else like 0x03 or 0x04. Is there any document which mentions that if we have to work on this board then 0x02 has to be used as phy address.

 

Can you please also tell that how this particular MAC address is chosen? same is it given in some document ?

0 件の賞賛
返信

1,984件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @achal ,

PHY address is determined by PHY address config pins on the PHY chip. Please refer to the EVK board.

jingpan_0-1687679001677.png

 

MAC address is random in the demo. Officially it is allocated by IEEE (Institute of Electrical and Electronics Engineers), the last three bytes, the hexadecimal number AE-3C-40 represents the serial number of a certain network product (such as network card) manufactured by the manufacturer.

 

Regards,

Jing

0 件の賞賛
返信