Documentation or Examples of cJSON for SLN-ALEXA-IOT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Documentation or Examples of cJSON for SLN-ALEXA-IOT

1,308 Views
alfonso1
Contributor I

Hello,

I'm looking for documentation or examples of utilizing cJSON to parse Alexa skill messages on the SLN-Alexa-iot. I am trying to parse just 1 number for example when the user says I have 10 apples. I want to be able to capture the number 10.

Any help would be appreciated.

Regards,

Alfonso

Labels (1)
0 Kudos
Reply
1 Reply

1,281 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi  Alfonso Sanchez Arellano 

   Could you please also share some test results on your side, you mentioned: I am trying to parse just 1 number for example when the user says I have 10 apples.

   Please give me our test result about it.

   About the examples of the CJSON with the Alexa, you can refer to the SLN-ALEXA-IOT SDK code, which can be downloaded from this link:

Welcome | MCUXpresso SDK Builder 

 You can check the code under : SDK_2.7.1_SLN-ALEXA-IOT\boards\sln_alexa_iot\sln_voice_examples

 The related code contains the CJSON process code.

  For more details, please check the project related  readme.txt.

Wish it helps you!

If you still have questions about it, please kindly let me know.

Best Regards,

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply