DMA interrupt not triggered when transfer started from ISR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DMA interrupt not triggered when transfer started from ISR

ソリューションへジャンプ
2,956件の閲覧回数
jterrien
Contributor II

Hello

I am using an i.MXRT1024 Evk and MCUxpresso for programming. I need to transfert several bytes from a LPSPI to memory every time a GPIO goes low. The process of the received bytes should be done in the DMA channel major loop interruption. The processor is running under FreeRTOS. I am not able to start the transfert nor fire the DMA channel interrupt from the GPIO ISR. Please find below what I discovered so far:

1) When I am starting the DMA transfert from a task, everything is fine. DMA transfer started and DMA interrupt fired. I am using the LPSPI_MasterTransferEDMALite(LPSPI3, &g_m_edma_handle, &eDMA_masterXfer); function

2) When I am starting the DMA transfert whithin the GPIO interrupt using LPSPI_MasterTransferEDMALite(LPSPI3, &g_m_edma_handle, &eDMA_masterXfer); the transfer is not taking place nor the interrupt

3) If I am using the  code below extract everything is fine (transfer + completion interrupt) in a task but not within the GPIO interrupt. The transfer is started but not the major loop interrupt

DMA0->TCD[0].DADDR = 0x81E00000; //DADDR reset to beginning of Memory

EDMA_StartTransfer(g_m_edma_handle.edmaTxDataToTxRegHandle);

EDMA_StartTransfer(g_m_edma_handle.edmaRxRegToRxDataHandle);

LPSPI_EnableDMA(LPSPI3, (uint32_t)kLPSPI_RxDmaEnable | (uint32_t)kLPSPI_TxDmaEnable);

 

Could you please help me in starting the DMA transfer within the interrupt ISR and

generating a DMA channel major loop interrupt after the transfer. Thanks in advance.

Best regards, Jérémy

 

 

0 件の賞賛
返信
1 解決策
2,758件の閲覧回数
jterrien
Contributor II

Dear Mayliu

 

I finally found what was the problem. It came from the fact that I was mixing blocking SPI transfer and DMA transfer. My program is now working perfectly fine and I can switch on the fly between blocking and DMA transfer without problem.

 

Thanks a lot for letting me see some hope in solving my issue.

 

Best regards, Jérémy

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,925件の閲覧回数
mayliu1
NXP Employee
NXP Employee

Hi @jterrien ,

 

Thank you so much for your interest in our products and for using our community.

I did  a test for you, I can start the DMA transfer within the interrupt ISR and generating a DMA channel major loop interrupt after the transfer.

I merge SDK demo "evkmimxrt1024_igpio_input_interrupt" and "evkmimxrt1024_lpspi_edma_b2b_transfer_master". I use MIMXRT1024-EVK board.

When I press SW4 button, in this GPIO IRQ Handler, call LPSPI_MasterTransferEDMALite function , then I can see that the program can enter LPSPI_MasterUserCallback callback function. 

mayliu1_0-1742200292975.pngmayliu1_1-1742200340217.png

 

Wish it helps you.
If you still have question about it, please kindly let me know.

Wish you a nice day!

Best Regards
MayLiu

0 件の賞賛
返信
2,898件の閲覧回数
jterrien
Contributor II

Dear MayLiu

Thanks a lot for your prompt reply. Unfortuneatly, it does not work in my program. I started from the example lwip_ipv4_ipv6_echo. What I discovered is that even if I start the transfer from another task the interrupt is not triggered as well. I can see the clock the spi toggling for the correct number of bytes (28 in my program) but the DONE bit in the TCD is never set and thus the interrupt is not fired. The same occure if I do the whole initialisation of DMAMUX, DMA and DMA channel (extract below) at each pin interrupt. I do not know if running FREERTOS might be the cause of the problem or not. Just in case if it can help I attached the main C and ADS1299_HAL files.

The start of the DMA transfert is done in the function ActivateDMA (ligne 490) of ADS1299_HAL.c.

The pin interrupt is handled in the function void GPIO1_Combined_16_31_IRQHandler(void) ligne 565 in the same file. It raises the NeedActivateDMA = 1; flag to signal to another task to call ActivateDMA().

Thanks for your help.

Best regards, Jérémy

This is the fonction ActivateDMA()

DMAMUX_Init(DMAMUX);

 

DMAMUX_SetSource(DMAMUX, LPSPI_MASTER_DMA_RX_CHANNEL, kDmaRequestMuxLPSPI3Rx);

DMAMUX_EnableChannel(DMAMUX, LPSPI_MASTER_DMA_RX_CHANNEL);

 

DMAMUX_SetSource(DMAMUX, LPSPI_MASTER_DMA_TX_CHANNEL, kDmaRequestMuxLPSPI3Tx);

DMAMUX_EnableChannel(DMAMUX, LPSPI_MASTER_DMA_TX_CHANNEL);

/* EDMA init*/

EDMA_GetDefaultConfig(&userConfig);

userConfig.enableDebugMode = true;

EDMA_Init(DMA0, &userConfig);

/*Set up lpspi master*/

memset(&(lpspiEdmaMasterRxRegToRxDataHandle), 0, sizeof(lpspiEdmaMasterRxRegToRxDataHandle));

memset(&(lpspiEdmaMasterTxDataToTxRegHandle), 0, sizeof(lpspiEdmaMasterTxDataToTxRegHandle));

EDMA_CreateHandle(&(lpspiEdmaMasterRxRegToRxDataHandle), DMA0, LPSPI_MASTER_DMA_RX_CHANNEL);

EDMA_CreateHandle(&(lpspiEdmaMasterTxDataToTxRegHandle), DMA0, LPSPI_MASTER_DMA_TX_CHANNEL);

LPSPI_MasterTransferCreateHandleEDMA(LPSPI3, &g_m_edma_handle, LPSPI_MasterUserCallback, NULL, &lpspiEdmaMasterRxRegToRxDataHandle, &lpspiEdmaMasterTxDataToTxRegHandle);

LPSPI_MasterTransferPrepareEDMALite(LPSPI3, &g_m_edma_handle, kLPSPI_MasterPcs0);

/* Start master transfer, receive data from slave */

eDMA_masterXfer.txData = NULL;

eDMA_masterXfer.rxData = eDMA_masterRxData;

eDMA_masterXfer.dataSize = 28;

CS1Low();

isTransferCompleted = false;

//Modifier to not generate transfer at spi level

LPSPI_MasterTransferEDMALite(LPSPI3, &g_m_edma_handle, &eDMA_masterXfer);

LPSPI_EnableDMA(LPSPI3, (uint32_t)kLPSPI_RxDmaEnable | (uint32_t)kLPSPI_TxDmaEnable);

タグ(3)
0 件の賞賛
返信
2,841件の閲覧回数
mayliu1
NXP Employee
NXP Employee

Please refer to my previous post, I am sure It can work. 

When you can realize what I did, you can merge the code to your project.

Please try it.

Thanks

0 件の賞賛
返信
2,759件の閲覧回数
jterrien
Contributor II

Dear Mayliu

 

I finally found what was the problem. It came from the fact that I was mixing blocking SPI transfer and DMA transfer. My program is now working perfectly fine and I can switch on the fly between blocking and DMA transfer without problem.

 

Thanks a lot for letting me see some hope in solving my issue.

 

Best regards, Jérémy

0 件の賞賛
返信
2,745件の閲覧回数
jterrien
Contributor II
Thanks
0 件の賞賛
返信