Custom bootloader imxrt1170

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Custom bootloader imxrt1170

1,055件の閲覧回数
burhanhagi
Contributor V

I am trying to port already existing boot firmware from STM platform to IMXRT platform. 

I have 2 QSPI Flashes. First one is executing the code only and the second is for storing some data.

I am also trying to add boot firmware to the second one. Every boot time, I will start to run from the second QSPI flash. If no new firmware is upgraded/loaded within a pre-defined time interval, I will start to execute main app program in first QSPI. At that time I am also trying to force second QSPI flash to "read/write" mode thereafter. However I could not find a way how to do that. Can you give me any example or show me a way of doing it?

0 件の賞賛
返信
1 返信

1,028件の閲覧回数
Littell
Contributor III

As they say, "Good luck with that."  Hopefully this will help some: https://www.nxp.com/docs/en/application-note/AN12564.pdf

0 件の賞賛
返信