CRC-32 using DCP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CRC-32 using DCP

3,462 Views
gary_metalle
Contributor III

Is it possible to configure the DCP block for different flavours of CRC?

From this link it appears the configuration is:

/* Expected CRC-32 for the message.
     * CRC-32 params:
     * width=32 poly=0x04c11db7 init=0xffffffff refin=false refout=false xorout=0x00000000
     * http://reveng.sourceforge.net/crc-catalogue/
     */

But I would like to use:

width=32 poly=0x04c11db7 init=0xffffffff refin=true refout=true xorout=0xffffffff

Well I say that... I think I do anyway if you follow the reveng link above for the CRC-32/ISO-HDLC variant which is what I already have a software implementation for.

If you run "12345678" through ISO-HDLC you will get a crc of 0x9ae0daaf but when I run it through the DCP I am getting 0xF954FCFE.

There is a 'swapConfig' field in the dcp_handle_t struct that looks promising but people always seem to set it to kDCP_NoSwap and I am not sure what kDCP_InputByteSwap and others are used for.

I've just run a quick test for SHA1 as well and that also doesn't match what I am expecting.

Tags (5)
0 Kudos
Reply
1 Reply

3,418 Views
JasonGT93
Contributor II

Hi Gary,

Did you find some information for this?

I posted similar question in this topic:

https://community.nxp.com/t5/i-MX-Processors/iMXRT1024-DCP-CRC-32-parameter-settings/m-p/1472829#M19...

Unfortunately I did not get any reply.

Best regards.

0 Kudos
Reply