CAN1 using in iMXRT1170 EVKB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CAN1 using in iMXRT1170 EVKB

跳至解决方案
560 次查看
D_D97
Contributor II

Hello, 

I'm using the " iMXRT1176DVMAA" microcontroller - iMXRT1170 EVKB to implement the CAN Bus functionality.

I used CAN3 and it worked fine, there were two jumpers to remove  ( j102 & j103 )
and now I don't know if there are any jumpers or resistors to remove before using CAN1.

Any help ? 

Thank you.

0 项奖励
回复
1 解答
489 次查看
mayliu1
NXP Employee
NXP Employee

Hi @D_D97 ,

Thank you for your interest in the NXP MIMXRT product, I would  like to provide service for you.

I did a test, I connect MIMXRT1170-EVKB board CAN1(J83) and MIMXRT1050-EVKB board  CAN2(J11),  CAN communication works normally. So I think you can refer to what I do.

1.png2.png

For hardware modification, you need to mount   R2057 and R2058.

3.png

 

For software, you need set CAN1 pins.  You also need modify some code based on CAN1.

4.png

 

Wish it helps you.
If you still have question about it, please kindly let me know.

Wish you a nice day!

BR

MayLiu

在原帖中查看解决方案

0 项奖励
回复
1 回复
490 次查看
mayliu1
NXP Employee
NXP Employee

Hi @D_D97 ,

Thank you for your interest in the NXP MIMXRT product, I would  like to provide service for you.

I did a test, I connect MIMXRT1170-EVKB board CAN1(J83) and MIMXRT1050-EVKB board  CAN2(J11),  CAN communication works normally. So I think you can refer to what I do.

1.png2.png

For hardware modification, you need to mount   R2057 and R2058.

3.png

 

For software, you need set CAN1 pins.  You also need modify some code based on CAN1.

4.png

 

Wish it helps you.
If you still have question about it, please kindly let me know.

Wish you a nice day!

BR

MayLiu

0 项奖励
回复